Part Number: HD3SS3212-Q1
Hello team,
I would like to check about the SEL pin on the HD3SS3212-Q1.
In the data sheet circuit example (Figure 13), CC Controller is connected, but I don't need such a function to detect the current supply capability of the host, so I am considering the circuit that detects the voltage on one side of CC pin of Type C connector and controls the voltage on SEL pin.
The schematic is as shown in the internal link, is it OK to use the SEL pin like this?
https://tidrive.itg.ti.com/a/Ceht6hZobfAb6G36/c0177f21-6591-45c5-971c-fca52536c83f?l
Regards,
Itoh