Part Number: TL16C750
Dear TI Team
Our customers are considering TL16C750FN (PLCC package) or TL16C750PM (LQFP package).
However, they are concerned about the availability and EOL potential of these products.
I want you to answer the following questions.
1. Which is in demand worldwide, the TL16C750FN or the TL16C750PM?
(Which one has the larger supply?)
2. Since I think the LQFP package is newer than the PLCC package, I recognize that the TL16C750PM is less likely to be an EOL than the TL16C750FN in the future.
Is the above recognition correct?
Best Regards,
Y.Ottey