Hi team,
customer use 960 with one 913A in project, the processor is TDA4. for TDA4 and 960 is TI demo board. they found they can't receive the sensor image data.
before, with the same 913A&sensor module, customer use 964 can reveive image data properly. I checked reg config, not found mistakes.
In the datasheet of 960, only find it compatble 953-Q1/935-Q1/933-Q1/913A-Q1, does it not support 913Q?
In 964, it compatible both 913 Qand 913A.
customer use 960 pattern mode, TAD4 can receive data normaly.
I attached reg setting, please help to check and confim if the 960 can support 913? what the difference between 913 and 913A?
For 913A &960, below is customer reg setting, please help to check if there need to change. I search on E2E find below link, if fixed issue but I'm not understand why need change 0x70 to1E and 0x7C[7:6] to 11.

thanks