Part Number: TCA8418
Other Parts Discussed in Thread: LM8330, LM8333
Hi,
We are planning to use TCA8418 to connect a 4 x 4 membrane keypad matrix switches.
With respect to debounce logic implementation, we have following observations:
1. First page of the device datasheet under feature section "Integrated Debounce Time of 50 μs" is specified, whereas in section 6.9 Keypad Switching Characteristics, maximum debounce time is mentioned as 60ms. So what is difference in these two debounce timing specs. please clarify?
2. As of now, we don't have the final specs of 4x4 membrane keypad switches, so in general, can we able to detect the membrane keypad switch cleanly if their debounce time is less than 60ms? In general, do you have idea what is the debounce time required for the membrane switches?
3. Do you have any other keypad scan IC to interface membrane matrix switch with adjustable/programmable debounce time?
4. Can we use external discrete components, usually a lo pass filter combination of R & C to increase the debounce time of the TCA8418?
Thanks & Regards,
Rajesh Kumar