This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849IF: DP83849IF ESD test failure

Part Number: DP83849IF


Hello,

One of my customer did touched 8KV Discharge experiment on Ethernet interface's RJ45 shell. It seems that DP83849IF is easy to failure on the test. The customer used a multimeter to measure the impedance of  Ethernet differential line to GND. The impedance is only 82 Ohm. and the impedance between differential line achieve 0 Ohm. Normally, the impedance of  Ethernet differential line to GND is around 580Ohm. I can send you the customer's schematic via email. Do you mind giving me some advices on it?

Many thanks for your help!

Best regards,

wenting +