Part Number: TUSB522P
Hello all,
I have system, which consist from two board and they are connector by 0.8 FFC cable:
I was afraid, that FFC cable will not pass USB3 signal, so i decided to use two Re-Drivers from each side of this cable
After many testing iteration, i found, that this setup work only with 0.4 or 1.0m FFC cable from one manufacturer and with 0.8m long FFC cable - won't work. No matter what redriving setting I use.
One note - with 1m FFC cable, i have working system system with 1m USB cable and even with 3m - still system working.
But, if I added external USB3 hub between PC and the USB cable - the system work with 0.8m long FFC cable (the redriving settings are at low settings). What are the difference between host controller and hub controller?
Maybe I can safely remover second Re-Driver form board2?
Thank for any kind of responses!