Part Number: DP83867IR
Other Parts Discussed in Thread: DP83869
Hi,
I want to connect 2 DP83867IR on the same PCB (with Gbit link). The design required a certain insulation between the PHYs. My questions are:
1. it is ok to have short distance between the PHY's (less than 50mm PCB traces)?
2. given the fact that the Ethernet transformer is not symmetrical (even if is 1:1 ratio - but use triple core configuration) it's ok to use only a single transformer (instead of 2) to connect the 2 ports?
3. the chipset does support capacitive coupling between the ports?
Thanks,
Best Regards,
Andrei