This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC811S-Q1: T5.2 and osc questions

Part Number: DP83TC811S-Q1


Hi Team.

May I ask two questions?

Is T5.2 time difference between VDDIO and VDDA?

Whether this osc is situable for 811?

SJK-7U25000MBZ1420B2--20101338.pdf  

  • Hello Amelie,

    Amelie Zheng said:
    Is T5.2 time difference between VDDIO and VDDA?

    Yes, T5.2 is the time difference between when VDDIO and VDDA cross 50% of their intended voltage level.

    Amelie Zheng said:
    Whether this osc is situable for 811?

    We would recommend a device that has a 50 Ohm ESR or lower. This is due to concerns that the oscillating system may not start up. More information can be found in section 3.8 here.

    Sincerely,

    Gerome