This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: schematic review

Part Number: TUSB4020BI

Hi team,

could you help review below schematic? we didn't need OCP function. thanks.

  • Hi Betty,

    Schematic feedback:

    Do not install pullups on PWRCTL/BATEN - doing so will enable battery charging mode.  Just allow them to float if not used.

    USB_VBUS is a detection input, it should only be high when an active host is connected upstream of the hub.

    GRSTz, a cap of 1 uF is sufficient for most applications, some applications require 2uF if the power on voltage ramps slowly.

    Regards,

    JMMN