Part Number: PCA9306
Other Parts Discussed in Thread: TXS0102
Hello Team,
does it work the PCA9306 for UART applications?
In this case the pull up resistors on SDA/SCL would not be present.
For UART would be TX and RX channel.
From the datasheet I do not see anything preventing it.
Can I use only one channel and use the second one floating?
I'm also considering the TXS0102 since it integrates the pull up resistors and does not need the external resistor for Vref.
The reason behind the question is due to the fact that connecting the systems on the PCA9306, we do see that the 0V pulled from one system (1.8V side) does not go low on the 3.3V side. We are able to pull it down till 0.3V which sounds like an ESD diode ON. Thus the question on the must to have the pull up resistor.
We are still investigating on the current that really flows, and if the 1.8V system is really capable of pulling low the line.
Thanks for the follow up.
SunSet