Part Number: TPD4E05U06
I plan to do SI Sim for USB3.2 gen1.
Can you provide the Sparameter for TPD4E05U06?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD4E05U06
I plan to do SI Sim for USB3.2 gen1.
Can you provide the Sparameter for TPD4E05U06?
Hello,
Thank you for using E2E! The S-Parameters model for this device is located on the product page under the "Design Tools & Simulation" section.
Regards,
Matt
I checked the Sparameter, but it was a 2port Sparameter.
Is it okay to recognize that this is Spara for 1Ch of TPD4E05U06?
Should I use port1 as an input and port2 as an output?
Hello,
Yes the 2 port model should work for the 1 channel device. Port 1 will be the input and port 2 will be the output.
Regards,
Matt Smith