Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
I want to convert 100 base-TX and 100 base-FX with DP 83869 HM. (Use as a Media Converter)
I set strap as follows.
However, it cannot communicate well.
*Datasheet Table 12. Functional Mode Strap Table
JTAG _ TDO/GPIO _ 1 (OPMODE _ 0) 1
RX _ D3 (OPMODE _ 1) 0
RX _ D2 (OPMODE _ 2) 1
*Datasheet Table 17. 100 M Media Convertor Strap Table
LED _ 1 (ANEGSEL _ 0) 0
LED _ 2 (ANEGSEL _ 1) 0
RX _ CTRL (MIRROR _ EN) 0
RX _ CLK (LINK _ LOSS) 0
What are the factors? (Register setting, etc.)
When the output signals from the SON and SOP jacks were observed with an oscilloscope, 1.25 Gbps signals were output. Does it work as SGMII or 1000 BASE-X?
If you look at "1.7 100 Mbps Media Converter" in the following URL, the setting of LED _ 1 and LED _ 2 is shown only in [1]. Should LED _ 1 and LED _ 2 be set to [1]?