Part Number: TPD2EUSB30
I have a customer wanting to use a single ESD device for multiple applications.
Can this device be used in any of the following applications? Are there any extra design concerns...?
- USB3.0
- DP
- LVDS
- Ethernet
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPD2EUSB30
I have a customer wanting to use a single ESD device for multiple applications.
Can this device be used in any of the following applications? Are there any extra design concerns...?
- USB3.0
- DP
- LVDS
- Ethernet
Hello Darren,
Yes this device should be able to provide protection for all of these applications. I don't believe any of the interfaces listed goes above 5.5 V, and the capacitance is low enough to where it can support all of the signal speeds (up to 7.4 Gbps). However, for the lower voltage interfaces like LVDS, which has a working voltage of around 1.25 V, you could use a device with a lower Vrwm like TPD1E01B04. This would allow you to get better protection.
Let me know if you need anymore clarification.
Regards,
Matt Smith