Hi team,
My customer plan to use DS125DF111 for 155M/622M/10.709G data rate.
Can DS125DF111 support as low as 155M/622M data rate? How to configure the registers?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer plan to use DS125DF111 for 155M/622M/10.709G data rate.
Can DS125DF111 support as low as 155M/622M data rate? How to configure the registers?
Hi,
10.709Gbps is supported in retimed mode. Refer to the programming guide Section 3.10 for instructions for implementing CDR manual mode configuration.
155M and 622M data rates are supported using CDR bypass mode. See below register write routine taken from the programming guide.
Table 1. Bypass CDR
STEP |
SHARED/CHANNEL REGISTER SET |
OPERATION |
REGISTER ADDRESS [HEX] |
REGISTER VALUE [HEX] |
WRITE MASK [HEX] |
COMMENT |
1 |
Channel |
Write |
0 |
04 |
04 |
Reset channel register to default. |
2 |
Channel |
Write |
09 |
20 |
20 |
Enable override output mux use reg_0x1e. |
3 |
Channel |
Write |
1E |
00 |
E0 |
Output raw data. |
Table 2. Bypass CDR (continued)
STEP |
SHARED/CHANNEL REGISTER SET |
OPERATION |
REGISTER ADDRESS [HEX] |
REGISTER VALUE [HEX] |
WRITE MASK [HEX] |
COMMENT |
4 |
Channel |
Write |
3F |
80 |
80 |
Disable fast research for refmode 3. |
5 |
Channel |
Write |
31 |
00 |
60 |
Set adapt mode to 0. |
6 |
Channel |
Write |
3A |
00 |
FF |
Set EQ boost value as 0. |
7 |
Channel |
Write |
40 |
00 |
FF |
Set EQ boost value as 0. |
8 |
Channel |
Write |
03 |
00 |
FF |
Set EQ boost value as 0. |
9 |
Channel |
Write |
2D |
08 |
08 |
Enable overriding the EQ setting from 0x03 register setting(Need to set for DF111s). |
10 |
Channel |
Write |
A |
0C |
0C |
CDR Reset. |
11 |
Channel |
Write |
A |
00 |
0C |
Release CDR Reset. |
Cordially,
Rodrigo Natal
HSSC Applications Engineer