Other Parts Discussed in Thread: DS90UB953-Q1,
Hi TI members:
I get one Sony IMX490 Camera Module (with use DS90UB953-Q1 serializer).
And our customer board have one DS90UB962-Q1 Deserializer.
So I try to connect IMX490 to DS90UB962.
Right now, Our EE let DS90UB962 FPD-Link's Vpoc output is 10V / 0.3A.
After I connect camera module to DS90UB962-Q1,
I change belw DS90UB962 register value,
i2cset -f -y 3 0x34 0x01 0x02 i2cset -f -y 3 0x34 0x4C 0x01 i2cset -f -y 3 0x34 0x58 0x5E i2cset -f -y 3 0x34 0x5C 0x18
After this, I can see 0x5B register value is auto loaded as 0x30.
Please see below register dump value
root@j7-evm:~# i2cdump -y -f 3 0x34
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: 68 00 1e 40 d0 01 00 fe 1c 10 7a 7a 0f b9 00 ff h.?@??.???zz??..
10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 04 02 ..............??
20: f0 03 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ??..............
30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
40: 00 a9 71 01 00 00 20 00 00 00 00 12 01 10 02 00 .?q?.. ....????.
50: 00 00 00 04 00 00 00 00 5e 00 00 30 18 00 00 00 ...?....^..0?...
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 7a 88 88 .............z??
70: 2b 2c e4 00 00 00 00 c5 00 01 00 00 20 00 00 00 +,?....?.?.. ...
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
a0: 00 00 00 00 00 1f 00 00 00 00 00 00 00 00 00 00 .....?..........
b0: 1c 3a 15 08 25 00 18 00 aa 33 83 74 80 00 00 00 ?:??%.?.?3?t?...
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
d0: 00 43 94 02 60 f2 00 03 00 00 00 00 00 00 00 00 .C??`?.?........
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 ................
f0: 5f 55 42 39 36 30 00 00 00 00 00 00 00 00 00 00 _UB960..........
So far I think I should can use SER_ALIAS_ID to access DS90UB953
But I failed, no matter I use i2cdetect or i2cdump, the slave address 0x0C all have no response.
Does I miss any register config?
BR
Sentinen Chen