Part Number: DP83TC811R-Q1
Other Parts Discussed in Thread: DP83TC811
Datasheet for Pin 5 says the following:
<<
Reference Clock Input (RMII): Reference clock 50-MHz CMOS-level oscillator in RMII Slave mode.
Reference clock 25-MHz crystal or oscillator in RMII Master mode.
>>
I have both, a master and a slave interface in RMII mode on the board, both controlled with 50 Mhz. Datasheet says that master-mode requires a 25 Mhz clock. Could that be why I have problems with the PHY? I am not completely sure how to understand the datasheet because I could also configure both PHYs as RMII via boostrap and then set one of them via SMI to master? If that is the case do I have to change/switch the oscillator input of the PHY, or is that not allowed? And do I have to aoways provide 25 Mhz to pin 5 on the master PHY?
Thank you!