Part Number: SN65DP159
・ Is it possible to switch the OUTPUT side?
・ Is it possible to use polar SWAP?
(Is it possible to use polar SWAP because there is no SWAP / POL pin even if I use 0x09h bit6 with I2C?)
-Is it only set in I2C (register 0x09h) for SWAP? Is it not possible to set externally?
・ Are the only specifications that can be swapped? If SWAP is set, is it possible to use only a part of this SWAP? (For example, SWAP only CLK and D2. D0 and D1 are noSWAP)