Part Number: DP83822I
Dear TI Team
I would like to ask about crystal spec of DP83822I.
The recommended crystal specifications in the data sheet are described in 10.2.2.1.1.2 below,
but the capacity specifications are also described in Table.144 25MHz Crystal Specification.
Is it okay to recognize each of these specifications as follows?
1.Crystal load capacity: 20pF recommended
2.CL1 and CL2 specifications: For 25MHz, 10-40pF (listed in Table.144) is recommended (check with the vendor for details)
Best Regards,
Y.Ottey