Hi Team,
My customer is using TCAN4550. But they recently found part of the devices cannot access its registers through SPI.
They checked the crystal input and output and discovered the jitter is very high with the `bad` one.
They PCB trace connecting crystal PIN1 and PIN3 is not at the same length. One is 2.5mm longer than another.
Could you help to estimate if the trace of crystal cause such communication issue?
Is there any specific requirement on crystal of TCAN4450?
Here is customer schematic:
Here are two waveform figures of PIN1 and PIN3 on the communication issue board.
Here is waveform of crystal output with `good` communication board.
B.R
Paul