Part Number: SN65HVD73
Hello team,
There is the difference between fig37 and fig41 for placing termination resistor.
I believe SN65HVD73 should be placed termination resistor at both Tx and RX. Is my understanding correct ?
And termination resistor should be placed closer to device as possible as they can but it should be placed in front of series resistor of ⑦ as datasheet ?
Is the pull-up resistor at R pin mandator ?
Customer believe it is not needed if SN65HVD73 has failsafe function.
Is the series resistor mandator when if RE pin and DE pin tied to VCC or GND directly.
In the fig41, the resistors limit noise current at transient situation but customer would like to make sure if it is mandatory or not.
Thank you and best regards,
Michiaki