Part Number: DP83869HM
Other Parts Discussed in Thread: AM3358, DP83869, DP83869EVM, USB-2-MDIO
Hi,
question 1: the DP83869HMRGZT pin43 is the RESET_N, I don't see the WPU (internal pull up) for this pin, so do I need adding a external pull up resistor( which connect to the VDDIO) to this pin?
question 2: this chip has two VDDA2P5 pins , three VDD1P1 pins, and two VDDIO pins, each pin should add the 1uF and 0.1uF decoupling capacitors, but in the datasheet page 109, Figure 114,DP83869HM power pins.docx, it showed there are three VDDIO pins, and four VDDA1P1 pins, can you explain why?
thanks,
Li