Part Number: TPS65987DDJ
Hello,
I would like to know if it is possible to use on the GPIO 0 and 21 the event Barrel Jack Detect Event ?
best regards
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65987DDJ
Hello,
I would like to know if it is possible to use on the GPIO 0 and 21 the event Barrel Jack Detect Event ?
best regards
David
Hi David,
Yes you may connect the Barrel Jack Detect GPIO event to both GPIOs. However, just remember that this event sets the GPIO as an input and will trigger when the barrel jack is connected. Therefore, to trigger this event you will need to connect both GPIOs externally to a signal that will go high when the barrel jack is inserted.
Thank you,
Hari