This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: 1% failure rate when writing 0x02 to 0x01 register after power up

Part Number: DS90UB953-Q1


Hi Team,

It's found that there is about 1% failure rate when writing 0x02 to 0x01 register of 953 after power up, because the GPIO1 is not pulled up and the sensor connected with 953 is not powered up, but the registers 0x0E and 0x0D are all configured successfully.

However, if 953 is not reset after power up, the sensor can always work normally.

So my questions are:

1. What will happen when writing 0x02 to 0x01 register of 953? Is there any unexpected effect by doing so?

2. Should 953 always be reset after power up? Per my understanding, it's not necessary to have 953 reset because 953 will go to default settings after power up.

Thanks and Best Regards!

Hao