Part Number: DS90UB941AS-Q1
Hi team,
we have two quesiton on DS90UB941AS-Q1:
1.RST_PLL_FREQ
could you help us understand the Reset mechanism on RST_PLL_FREQ? how much frequency change will triggle PLL be reset? if we set this bit to 0, is there any protential risk on product design?
2. SPLIT MODE Usage:
Customer is working on evluate the SPLIT MODE of DS90UB941. The requirement is to use this serializer to output two wires to DS90UH948 as the deserializer for two identical displays.
Current problem: There is no problem when 941 drives only one screen. When set to split mode, the i2c register of 948 cannot be accessed, but the link status of 948 is normal.
Support need: could you help provide us with the pseudo-code for the demo configuration of split mode; currently this way to drive two exactly the same screen is supported (the screen is developed by a third party, its configuration is exactly the same, and the i2c address is also the same)
BR
Brandon