Hi, Team,
2 questions below,
- Is the internal pulldown circuit activated in between "IC powered ON and GPIO settings"?
- Isn't the internal pulldown circuit activated before IC powered ON?
Thanks,
Best regards,
Koh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Team,
2 questions below,
Thanks,
Best regards,
Koh
Hello Koh,
before releasing PDB, GPIO pins are Tri-state.
Hi, Hamzeh,
Thanks for the reply.
How is this question?
The default is set as INPUT port for all GPIOs. This case those pins are pulled down once PDB released?
Then after change the register settings for OUTPUT enabled, how is operated an internal pull down circuit?
Best regards,
Koh
Hello Koh,
By default, the GPIO pin is enabled as input and the internal pulldown resistor in the GPIO is enabled. If you change the GPIO to output, the internall pulldown will be automatically disabled.