Part Number: TPS65988DJ
Other Parts Discussed in Thread: TPS65988
Hi,
It is shown in the datasheet of TPS65988, LDO 3V3 output is connected to VIN 3V3 by a single directional switch. All SPI and I2C lines are pulled up with LDO 3V3 output which should be the same when VIN 3V3 present. We have dedicated 3V3 system power and can I directly connect SPI and I2C pull ups 3V3 rather than LDO 3V3 output? Is there any side effect of connecting SPI and I2C pull ups directly to 3V3 rather than LDO 3V3 output?
Finally, it is recommended to connect I2C2 lines to pull-up resistors even we don't use them. Could you please let me know what is the adverse effect can be seen if I2C2 lines are not connected to pull-up resistors?
Many Thanks & Regards;
Mehmet