Part Number: TPD1E01B04
Other Parts Discussed in Thread: ESD122
Hi expert,
Does TPD1E01B04 can be used to protect 10G Ethernet port?
Detail specification requirement as below. I didn't find a device that can meet all these requirement. what's the bext recommendation for this case?
1、2-Line Surge and ESD Protection
2、Low Capacitance: 0.25pF Typical
3、Working Voltage: 3.3V
4、Very Small PCB Area
5、Transient Protection to
CE IEC 61000-4-2 (ESD) 25kV (Air), 25kV (Contact)
CE IEC 61000-4-4 (EFT) 4kV (5/50ns)
CE IEC 61000-4-5 (Lightning) 10A (8/20μs)