Part Number: TPS25850-Q1
Other Parts Discussed in Thread: TPS25831-Q1, TPS25833-Q1
The datasheet for this part gives Abs Max input voltage (IN to PGND) as 40V.
This part would be ideal for my application but the nominal supply voltage I have to deal with is 28V allowing for 36V transients.
The recommended operating voltage for the part is given as 26V so it becomes unsuitable for my application, unless the 26V is a typo and it should read 36V.
What is the reason behind such a large difference between recommended and abs max please as it is >50% of the recommended which is unusually high?
Many thanks