Hi,
I am flashing the external memory on the TPS65988EVM with the Application Customisation Tool v6.1.1 and I am seeing different results when using the 'Flash from binary file' and the 'Flash from current project' options. My scenario is this one:
1. Start a project
2. Save full binary 0x2000, 0x9000 as 'full.bin'
3. Flash from Project. Read binary
4. Flash from 'full.bin'. Read binary
The binaries from step 3 and 4 have differences around the region header area of both regions. Could you explain why this is the case?