Part Number: DP83640
Hello
We are using DP83640 Ethernet PHY with a custom board, based on am335x soc with RGMII connection (PHY is in master mode - i.e. recevies input from 25Mhz crystal to produce 50Mhz output) and we experience issues.
What we have so far:
1. Internal loopback test between MAC and PHY works (i.e. no errors, link is ok, all packets are received back)
2. External loopback does not work at all (phy does not detect itself - i.e. does not link to itself)
3. When connected to host PC PHY, the link is established (from MDIOLINK register and leds on the phy), PHY is able to receive data from pc (based on CPSW_STATS registers), but host pc does not receive anything (again CPSW_STATS registers on the board show that the data is being sent).
We use Transformerless Ethernet connection similar to the one described in SNLA088A TI application report.
I would appreciate if you could provide any help on how to resolve this issue.
Best regards,
Denis