Part Number: DS90UB941AS-Q1
FPD linkIII
Serializer DS90UB941, DSI
De-serializer DS90UB928 LVDS
Resolution: 720p
command setting:
{I2C_ADDR_MAIN, 0x01, 0x08, 0},
{I2C_ADDR_MAIN, 0x1e, 0x01, 0},
{I2C_ADDR_MAIN, 0x40, 0x05, 0},
{I2C_ADDR_MAIN, 0x41, 0x21, 0},
{I2C_ADDR_MAIN, 0x42, 0x60, 0},
{I2C_ADDR_MAIN, 0x5b, 0x01, 0},
{I2C_ADDR_MAIN, 0x4f, 0x8c, 0},
{I2C_ADDR_MAIN, 0x40, 0x04, 0},
{I2C_ADDR_MAIN, 0x41, 0x05, 0},
{I2C_ADDR_MAIN, 0x42, 0x0a, 0},
{I2C_ADDR_MAIN, 0x5D, 0x3F, 0},
{I2C_ADDR_MAIN, 0x03, 0x9A, 0},
{I2C_ADDR_SLAVE, 0x1D, 0x25, 0},
{I2C_ADDR_SLAVE, 0x4B, 0x01, 0},
{I2C_ADDR_MAIN, 0x03, 0x92, 0},
{I2C_ADDR_MAIN, 0x01, 0x00, 0},
Issue:
LOCK of DS90UB928 is not stable when DS90UB941 lost DSI signal.(system suspend.)
Failrate: 9/60 pcs
Abnormal :
Normal: