This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83620: IBIS model selection

Part Number: DP83620

Hi,

In the DP83620 IBIS model, there are four models available

g24q370 mode: SS = VSS, VDD = 3.3
g24q371 mode: SS = VDD, VDD = 3.3
g24q372 mode: SS = VSS, VDD = 2.5
g24q373 mode: SS = VDD, VDD = 2.5

Since we are using 3.3V, the first two options will satisfy our requirement.

g24q370 mode: SS = VSS, VDD = 3.3
g24q371 mode: SS = VDD, VDD = 3.3

In our design, 100Mbps MII interface is used. How to select among these two models for our design?

Thanks

Viswa