Part Number: TCAN1051H
Other Parts Discussed in Thread: TCAN1051, TCAN1051-Q1
Hi team,
I met some problem when I used TCAN1051, could you please offer some advices for my issue?
- When the TXD=1 or no connection, the CANH=CANL=2.5V and it is normal.
- But When the TXD=0, the CANH CANL is still 2.5V which is wrong.
3. At first, I though that it was caused by the protection after the CANH and CANL, so I let the R50 and R49 to be NC, but the situation is not changed.
The schematic of TCAN1051 and protection circuit is shown below (by the way the R46,R47,R10,R11 is always NC).
Best Regards
Wesley Huang