Part Number: DS90UB933-Q1
HI Team,
In 8-bit parallel mode, is below setup ok and how to configure the device mode or registers?
DS90UB933 connects the lower 8-bit input(D0-7) and the DS90UB934 connects the upper 8-bit output(D2-9)?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
HI Team,
In 8-bit parallel mode, is below setup ok and how to configure the device mode or registers?
DS90UB933 connects the lower 8-bit input(D0-7) and the DS90UB934 connects the upper 8-bit output(D2-9)?
Thanks
Hi Ted,
This isn't supported because the mapping is 1-to1.
Best,
Jiashow