Hi Team,
I have some questions about UB960-Q1. Our application is using 953*2 + 960.
1. I2S Mapping
I see the SNLA314A which could use GPIO pin as I2S when using 953+954. Could we use the same method in UB960-Q1. We used two 953 and use 960 GPIO0-5.
2. CSI-2 Mode Virtual Channel Mapping question
Could we use below scenario by software register setting because we only use 2 camera?
Regards,
Roy