Part Number: TPS65988
Other Parts Discussed in Thread: BQ25611D, , BQ25703A
Hi,
I am considering the composition of the attached excel.
(question 1)
Regarding the configuration of ①, we are thinking of controlling the charging current according to the DCP, CDP, and SDP that can be discriminated by the charging IC.
The MCU can communicate via USB via the charging IC.
The charging IC can communicate with the MCU via I2C.
I think that the BQ25611D can distinguish SDP etc., but the MCU cannot do USB communication.
Is there a charging IC that can be used like ①?
(Question 2)
In the configuration of ②, the USB control IC can distinguish DCP, CDP, and SDP, and can notify the MCU.
The MCU can communicate via USB via the USB control IC.
The charging IC can change the charging current from the MCU by I2C control.
In this configuration, we are considering the TPS65988/87D as a USB control IC.
It seems that BQ25703A can be used as the charging IC, but is there any other charging IC that can be used?
I would be grateful if you could introduce me to an inexpensive charging IC.
Best regards,