Part Number: DP83867IR
Hi Experts,
My customer is facing an issue that the communication over ethernet does not work. PING cannot reach to peer device. Below is the detail.
- Once this failure occurs, user needs to plug out and re-plug in to restart it..
- The failure rate is once per 100 times of the cable plug-in. The failure rate seems to depends on the ethernet cable. This occurs when using CAT5 w/o shield. When using CAT5 WITH shield, the failure rate becomes lower.
- Auto negotiation ON, Auto MDIX
- The peer device is the switching hub and LINK LED is on even when this failure occurs.
- They dumps resisters and below are only differences.
|
Address |
NG |
OK |
|
ANER (0x0006) |
0x006F |
0x006D |
|
ADDAR (0x000E) |
0x00AA |
0x0000 |
|
ISR (0x0013) |
0x1C40 |
0x0000 |
Can you please suggest anything how to find the root cause?
Regards,
Uchikoshi