This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: MIPI CSI DISABLE LP MODE

Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP

Hi TI Support Team

I want to disable 954 mipi csi LP mode because i only want to verify the HS mode eye diagram. Can you please check how to implement it. 

From my side, i use the test pattern from ALP_Documents\PreDefScripts\DS90UB954 

e.g. 954_400Mbps_CSI.py ; 953to954_patgen_YUV_1920x1080p-4Lanes-Working.py ; 954_patgen_RGB888_colorbar_1920x1080p30.py

And i add the register 0x02 output_sleep_state_select bit 2 to 0, the CSI TX output will be forced into a HS-0 state. but it can't disable MIPI LP mode from the MIPI DATA signal. 

Thanks

Yutai