Part Number: TPS25750EVM
Other Parts Discussed in Thread: TPS25750, BQ25792, BQ25792EVM, , BQ25731
Hi,
We are implementing TPS25750 + BQ25792 for a sink only application with a power path management.
Could you provide guidance to connect TPS25750EVM with BQ25792EVM:
We have really limited info regarding the BQ25731 embedded in TPS25750EVM especially if its I2C slave address is the same as BQ25792 (6Bh)?
Hence, are we are forced to unsolder BQ25731 from the EVM if we want to do a setup with BQ25792EVM?
Also, could you confirm that for the final setup, we could directly flash the memory content from the EVM’s flash dump to our final equivalent design to get it working?
I want to be sure that the TPS25750 Application Customization Tool stores persistent data only in the companion EEPROM and there is no persistent operation performed on the TPS25750 itself.
Best regards!