Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
I am currently able to send 1000base-X full duplex fiber traffic between 2 DP83869 PHYs but I need to be able to go down to half duplex mode so only a single LC fiber cable is needed.
I have tried writing bit 8 of register 0x00 to 0 to enable half duplex mode but reading back register 0x11 bit 13, it would still report full duplex. Disconnecting any of the 4 fiber cables will stop a link/data from passing. I have a 2-to-1 fiber converter that I tried also and it seems that the receiver can still receive when a single cable is inserted but the TX seems to require RX to see a signal in order to send.