Part Number: DS90UB954-Q1
Hi,
We are using the 953->954 as serializer->deserializer and treaming two virtual channels from the same camera.
We are facing some problems in the host side of capturing the data so we need some help:
- In reg 0x21[7] we can 'CSI_REPLICATE' the stream, on which physical lines is that streaming out from the 954?
- Is there any possibility to see the status of VID -0 and VID-1 separately in one of the status registers of the 954.
Thx
Neta