Part Number: TCAN1042HGV-Q1
Hi TI Team,
We are facing an issue with Standby mode for TCAN1042HGV-Q1.
INFO:- VCC=VIO= 5V(Isolated). TX,RX,STB driven via Optoisolators.
As per datasheet, transceiver shall enter low power consumption when STB pin is pulled to VCC.
Observation:- The STB pin is pulled HIGH if it is left floating but remains LOW if we try to drive it using opto-isolator.
We are not disconnecting the VCC or VIO supply when we want to send the transceiver to standby mode.
Can this be an issue?
Regards,
Rohan