Part Number: DP83849I
Other Parts Discussed in Thread: TIDA-00306,
Hi Team,
For Table 7 – “Jumper Settings for TIDA-00306”, J51 and J56 are specified as “Strapped-high”. Yet, the jumper can only be present or not present, as these are only 2-pin headers. For other 2-pin headers, the table shows either “Strapped” or nothing at all. The other entries listed as “Strapped-high” relate to 3-pin headers, where the middle pin is the signal and the others are VCC and GND. In the case of J51 and J56, one pin is the signal and the other is GND. So, should I connect a wire to the signal and VCC (somewhere else on the board), or just leave these unjumpered?
Regards,
Ramon