Part Number: DP83867E
We are implementing the DP83867E. We have used it with RGMII before, now we want to use it in SGMII application. I don't understand how the strap configuration should be. This (attached) image is how we configured for RGMII. I got this reference from one of our companies recent projects. I assumed that I only needed to change the strapping configuration to have the PHY LED0 with resistors. Reading the datasheet had me completely confused.
1. what to do with unused pins,
2. Page 39 of the datasheet expresses two notes regarding RX_D3 and RX_D1 with SGMII, but I thought that those two pins are used in SGMII RX_D3 and RX_D1 are identified as SGMII_SOP and SGMII_SON, so why would they be strapped? TX_D2 & TX_D3 & RX_CTRL and RX_CLK pins, how do they get connected or not connected when in SGMII mode.