Part Number: TCA9801
Other Parts Discussed in Thread: TXS0102, PCA9306
Hi team,
My customer is considering TCA9801 or TXS0102. Could you support the questions below?
1. TCA9801 has only DGK package. Do you have a plan to develop small package like DCT, DCU, DQE, DQM, and YZP with TCA9801?
2. TXS0102 seems to have internal pull-up resistor 10kohm on both Ach and Bch. Could you tell me the accuracy of the pull-up resistor?
3. What is the difference in features between the TCA9801 and TXS0102?
4. Can you introduce another I2C level shifter with lower leakage current and smaller package other than TCA9801 and TXS0102 if you have?
Although the TXS0102 has a smaller leakage current than the TCA9801 and a smaller package, customer is concerned about the increase in system verification time due to the built-in pull-up resistor.
Regards,
Yamaguchi