Hi team,
My customer want to use our AM26C31, could you please share the ESD performance(HBM, CDM ) of the device? Also shared the reflow soldering peak temperature and Dwelling time on peak temperature?(260°C, 30s?). Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
My customer want to use our AM26C31, could you please share the ESD performance(HBM, CDM ) of the device? Also shared the reflow soldering peak temperature and Dwelling time on peak temperature?(260°C, 30s?). Thanks.
Frank,
The ESD performance for this device, both HBM and CDM, are located in the datasheet in the Absolute Maximum section. For soldering reflow, we recommend following the IPC/JEDEC J-STD-020D standard and the recommendations from the solder paste vendor.
For some more information from TI application notes:
MSL Ratings and Reflow Profiles (Rev. A)
Solder Pad Recommendations for Surface-Mount Devices (Rev. A)
Absolute Maximum Ratings for Soldering (Rev. D)
Please let me know if this helps, or if you need more information.
Regards,