Part Number: DP83822I
Hello Team,
the DP83822 MAC has series termination resistors.
The Table 79 specifies all the values I can set.
The datasheet only mentions that those impedance are for the MAC digital pins.
Since it is a series resistor I would assume that it is only for the output drivers and not for the input lines.
- Can you confirm which pin/lines do have the series Terminations?
- Pins that are In/Out (depending on the configuration), I'm assuming that also have the terminations on the output, once set as Out.
- Since the datasheet does not mention that you have to enable it, I take the assumption that by power up the impedance has the default value and then I can trim it as required by the application. can you confirm it?
Thanks,
SunSet