Part Number: DS90UB947-Q1
Hello,
My customer is considering sending PWM through DS90UB947/948 chipset. Because the PWM requires rather high resolution, its data rate or sampling frequency is higher the better. So, I would like to know how high it can be for the below 3 possible cases. Please make an answer to the below questions:
1. Standard GPIO (pin: 14, 15, 38, 39):
What is the sampling frequency?
2. High speed GPIO (pin: 43, 44, 45, 46):
What is the sampling frequency?
3. I2S (pin: 34, 35, 36)
In frame transport mode, can I2S_CLK pin used as highspeed GPI?
Or if not, with 13MHz clock being provided to I2S_CLK, can I2S_DA be used as 13MHz sampling GPI? My concern is it may have to be in I2S or TDM format.
Another question is what is the "CLK/2" in the below description in p.24 of DS90UB947 datasheet? Is it half the clock signal to CLK+/CLK- pins?
7.3.13.1 I2S Audio Interface
The DS90UB947-Q1 serializer features six I 2S input pins that, when paired with a compatible deserializer, supports 7.1 High-Definition (HD) Surround Sound audio applications. The bit clock (I2S_CLK) supports frequencies between 1MHz and the lesser of CLK/2 or 13 MHz. Four I 2S data inputs transport two channels of I 2S-formatted digital audio each, with each channel delineated by the word select (I2S_WC) input. Refer to Figure 21 and Figure 22 for I2S connection diagram and timing information.
Thanks.
Regards,
Oguri (TIJ automotive FAE)