Part Number: DS90UB962-Q1
Dear team,
My customer uses 962 paired with 933*4. The camera PCLK is 99MHz. The data format is YUV422 8bit. FPDLINK serial rate is PCLK*28/2=1.38Gbps. In my understanding, 962's CSI-2 lane speed should be set 1.6Gbps per lane which is larger than 1.38Gbps, but it still works normally when I set 800Mbps per lane, which is very strange. Is there any wrong with my computation?
Thanks & Best Regards,
Sherry