Hi,
I am using TCAN4550 to receive and transmit the CAN data.by default it is using RX FIFO0 only to stanks ore the received CAN messages.when i receive the CAN messages at 1ms frequency there is huge data loss.hence i want to use RX FIFO1 also along with RX FIFO0. How can i use both FIFO's simultaneously?what are the required configurations fr that?Please guide me.
Thanks in Advance,
Bipin